This tab shows the detailed information on projects (main project) categorized by the following and the configuration can be changed.
[Description of each category]
The detailed information on files is displayed.
| Displays the file name of the file to save the information on the main project. | ||||
| Displays the absolute path of the main project file to save the information on them. | ||||
| Type of storage and sharing environment-dependent information | Selects the method for saving and sharing an environment-dependent information-saving file (*.mtud). For details, see 2.10.5 Save and share environment-dependent information-saving files. | |||
| Depends on the setting of the [Set default value as "Share settings among users" to [Type of storage and sharing environment-dependent information] property on creating project] option for the [General - Project] category in the [Option] dialog box. | ||||
| The environment-dependent information is not saved. When you close a project, the information will be lost. | ||||
The detailed information on a license is displayed and their configuration can be changed.
The detailed information on records is displayed and their configuration can be changed.
| Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can use a text box directly enter the text. | |||