You can set whether toolbars are displayed or not, change toolbar names, and make new toolbars.
 
The following items are explained here.
Display a list of the names of registered toolbars.
A check mark appears in front of the name of the toolbar currently displayed in the Main window. By removing the check mark, you make a setting so that the toolbar will not be displayed.
| Opens the New Toolbar dialog box to make a new toolbar. The name of the new toolbar will be added to the list displayed in the [Toolbars] area with a check mark placed in front. Note that there are no buttons on the newly created toolbar. The register buttons on it, use the [Commands] tab. | |
| Opens the Rename Toolbar dialog box to change the name of the currently selected toolbar. This function is disabled when a toolbar other than those created by the user is selected. | |
| This function is disabled when a toolbar other than those created by the user is selected. | |
| Discards all changes made to the selected toolbar and returns it to the default state. When a toolbar created by the user is selected, this button returns the selected toolbar to the state with no buttons registered on it. | 
| Opens the Customize Keyboard dialog box to assign customized items to keys on the keyboard. | |
| Cancels the toolbar/menu customization settings and closes this dialog box. |