D.2  Displaying Icons at Locations of Input Errors
 
In some of the panels and dialog boxes provided by CS+, the  icon will appear at a point where incorrect characters are entered or a required item is missing.
 icon will appear at a point where incorrect characters are entered or a required item is missing.
| 
Remark | Placing the cursor over the  icon will pop up the information that indicates the characters to be entered (tips to fix the error). | 
| 
Figure D.1 | Sample Icons Shown at Locations of Input Errors |