The acquired floating license (offline mode) is automatically returned to the server when it expires. You can also manually end usage in offline mode and return the floating license before it expires.
When the client is connected to the server, click on the license name and the [Stop offline mode] button in the License Manager window.
A floating license (offline mode) is returned to the server, and the displayed information in the License Manager window is updated.