In the License Manager window, click on the [Add license] button, and enter a license key in the [Add following License keys] text box, then click on the [Add] button to add the license.
Figure 2.6 Add Node Locked License Dialog Box
To register an Upgrade (version) node-locked license (permanent), a node-locked license (permanent) must have been registered as the source of the upgrade. Start by adding the node-locked license (permanent) to the license manager or add the Upgrade (version) license and node-locked license (permanent) at the same time. |
The [SOFTWARE LICENSE AGREEMENT] dialog box appears if you need to agree to the license agreement for the addition of a node-locked license.
Select [Accept] and click on the [OK] button. The node locked license you have added is now available.