Everything
3.1 Message Types

The message types (1 alphabetic character) when Floating License is operated are as follows.

Table 3.1

Message Types

Message Type

Description

C

Internal error

Processing was terminated (suspended) due to an internal error.

E

Fatal error

Processing was terminated (suspended) due to a fatal error.

M

Information

Informational message. Check the message and continue the processing.

W

Warning

Warning message. Check the message and continue processing.