Everything
 

Breakpoint Setting dialog box [Full-spec emulator][E1][E2][E2 Lite][E20]


This dialog box is used to set the breakpoints that are to be registered to the Pseudo-Error Debugging panel [Full-spec emulator][E1][E2][E2 Lite][E20].

Figure A.59

Breakpoint Setting Dialog Box

 

This section describes the following.

[How to open]

-

On the Pseudo-Error Debugging panel [Full-spec emulator][E1][E2][E2 Lite][E20], click the [Set Breakpoint...] button on the toolbar.

[Description of each area]

(1)

[Address]

You can either enter an address expression of a breakpoint directly into the text box (up to 1024 characters), or select one from the input history via the drop-down list (up to 10 items).

[Function buttons]

Button

Function

OK

Registers the breakpoint set in this dialog box to [Breakpoint List] in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E2][E2 Lite][E20].

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.