Everything
 

Pseudo-Error Debugging panel [Full-spec emulator][E1][E2][E2 Lite][E20]


This panel is central to the functionality of the solution for pseudo-error debugging.

See "2.24 Pseudo-error Debugging [Full-spec emulator][E1][E2][E2 Lite][E20]" for details on the solution for pseudo-error debugging.

Figure A.57

Pseudo-Error Debugging Panel

 

This section describes the following.

[How to open]

-

From the [Debug] menu, select [Debug Solutions] >> [Pseudo-Error Debugging].

-

On the Solution List panel, click the [Pseudo-error Debugging] button of Pseudo-error debugging.

[Description of each area]

(1)

Pseudo-error list area

This area lists pseudo-errors which are targets in pseudo-error debugging.

The full name of a pseudo-error is displayed by hovering the mouse cursor over the node of each pseudo-error.

Each item is explained as follows:

(a)

Check box

When a check box is selected, this pseudo-error is generated after pseudo-error debugging starts.

(b)

Occurred

This column shows whether this pseudo-error has been generated when the debugger is stopped.

"!" is displayed if the pseudo-error has been generated and nothing is displayed if it has not been generated.

Remark

A bit is always assigned per error to indicate whether an error occurred. Two bits are assigned to some errors and the number of occurrences of an error that can be counted is up to three (e.g., this is the case for errors No. 0 to 7 in RH850/G4MH devices). If the pseudo-error has occurred several times, “!” will be displayed as the number of times the error has occurred. To check the number of bits that are assigned to an error, see “ECM Error Source Status Register” in the chapter of the ECM in User's Manual: Hardware for the MCU in use.

(c)

Error Name

The abbreviated name of this pseudo-error is displayed.

(d)

Bit Name

The bit name of IOR that triggers the generation of this pseudo-error is displayed.

(2)

[Breakpoint List]

A list of breakpoints that are to be used for pseudo-error debugging is displayed.

Only the breakpoints whose check box is selected will be valid for pseudo-error debugging.

Either of the following icons is displayed at the beginning of each breakpoint.

 

Breakpoint is valid.

 

Breakpoint is invalid.

[Toolbar]

 

Starts pseudo-error debugging based on the settings made in this panel.

 

Has the same functionality as the same button on the Debug toolbar in the Main window.

 

Opens the Select Pseudo-Error dialog box [Full-spec emulator][E1][E2][E2 Lite][E20] used to select ECM pseudo-errors that are targets of pseudo-error debugging.

 

Clears the error status of all pseudo-errors.

 

Opens the Breakpoint Setting dialog box [Full-spec emulator][E1][E2][E2 Lite][E20] to add a breakpoint.

 

Deletes breakpoints selected in [Breakpoint List].