Everything

2.4.6 Limiting range of usage status

On the Analysis Result panel, by dragging and dropping with the mouse cursor in the Execution transition display area in the Analysis information diagram area, the user can change the analysis information to be displayed in the Analysis information table area from "analysis information in the trace data acquisition period" to "analysis information in the analysis information extraction interval".
It should be noted that the background for the Analysis information extraction interval that appears when the mouse cursor is dragged and dropped in the Execution transition display area assumes the magenta color.
Figure 2-8. Limiting Range of Usage Status
Remark By scrolling the marks that are displayed directly below the Start time of analysis information extraction/End time of analysis information extraction, similar to the regular scroll bar, the user can change the Analysis information extraction interval.