Everything
Everything
top
with RI600V4
Analysis
FUNCTIONS
Clear Analysis Information
2.5 Clear Analysis Information
By pressing the
button located on the
Toolbar
on the
Realtime OS Task Analyzer panel
, the user can clear the analysis information that is displayed in the
Child-panel display area
.
Figure 2-9. Clear Analysis Information
Remark Pressing the
button also clears the contents of the trace buffer.
To the latest version of this page
Differences Information
Previous Topic
Limiting range of usage status
Next Topic
Save Analysis Information
Table of Contents
Overview
Open Realtime OS Task Analyzer Panel
Set Trace Start Event
Open Analysis Result Panel
Clear Analysis Information
Save Analysis Information
Restore Analysis Information