Serial interface UARTMG
Below is a list of API functions output by the Code Generator for serial interface UARTMG use.
Figure 3.55 API Functions: [Serial interface UARTMG]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the serial interface UARTMG.  | |
| 
       Performs user-defined initialization related to the serial interface UARTMG.  | |
| 
       Performs processing in response to the UARTMG transmission completion interrupt INTSTMGn.  | |
| 
       Performs processing in response to the UARTMG reception completion interrupt INTSRMGn.  | |
| 
       Perfomrs processing in response to the UARTMG reception error interrupt INTSREMGn.  | |
| 
       Sets UARTMG communication to standby mode.  | |
| 
       Ends UARTMG communication.  | |
| 
       Halts the clock supplied to the serial interface UARTMG.  | |
| 
       Starts UARTMG data transmission.  | |
| 
       Starts UARTMG data reception.  | |
| 
       Performs processing in response to the UARTMG transmission completion interrupt INTSTMGn.  | |
| 
       Performs processing in response to the UARTMG reception completion interrupt INTSRMGn.  | |
| 
       Performs processing in response to the UARTMG reception error interrupt INTSREMGn.  | |
| 
       Performs processing in response to detection of overrun error.  |