Sets the clock source.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_cgc.h"
MD_STATUS R_CGC_Set_ClockMode ( clock_mode_t mode );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       clock_mode_t mode;  | 
    
       Clock source type MAINCLK : Main clock oscillator SUBCLK : Sub-clock oscillator PLLCLK : PLL circuit HOCO : High-speed on-chip oscillator LOCO : Low-speed on-chip oscillator  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ERROR1  | 
    
       Exit with error (abend)  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument mode specification  |