Everything

Function Reference

This section describes the API functions output by the Code Generator, using the following notation format.

 

Figure 3.1  Notation Format of API Functions

 

(1)           Name
Indicates the name of the API function.

(2)           Outline
Outlines the functions of the API function

(3)           [Syntax]
Indicates the format to be used when describing an API function to be called in C language.

(4)           [Argument(s)]
API function arguments are explained in the following format.

I/O

Argument

Descripton

(a)

(b)

(c)

(a)      I/O

          Argument classification

          I         …   Input argument

          O       …   Output argument

(b)      Argument

          Argument data type

(c)      Description

          Description of argument

(5)           [Return value]
API function return value is explained in the following format.

Macro

Description

(a)

(b)

(a)      Macro

          Macro of return value

(b)      Description

          Description of return value