Performs processing in response to the comparator C interrupt.
Remark This API function is called to run interrupt processing for the comparator Cn interrupt, which is generated when the comparison result changes at this time.
[Syntax]
static void r_cmpc_cmpcn_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.