Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the start condition detection in response to calling of R_RIICn_Master_Receive.
Remark This API function is called as the r_riicn_error_interrupt callback routine.
[Syntax]
static void r_riicn_callback_receiveend ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.