Gets the result of conversion.
[Syntax]
#include "r_cg_s12ad.h"
void R_S12ADn_Get_ValueResult ( ad_channel_t channel, uint16_t * const buffer );
Remark n is the unit number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
ad_channel_t channel; |
Channel number ADCHANNEL0 : Input channel AN000 ADCHANNEL1 : Input channel AN001 ADCHANNEL2 : Input channel AN002 ADCHANNEL3 : Input channel AN003 ADCHANNEL4 : Input channel AN004 ADCHANNEL5 : Input channel AN005 ADCHANNEL6 : Input channel AN006 ADCHANNEL7 : Input channel AN007 ADCHANNEL8 : Input channel AN008 ADCHANNEL9 : Input channel AN009 ADCHANNEL10 : Input channel AN010 ADCHANNEL11 : Input channel AN011 ADCHANNEL12 : Input channel AN012 ADCHANNEL13 : Input channel AN013 ADCHANNEL14 : Input channel AN014 ADCHANNEL15 : Input channel AN015 ADCHANNEL16 : Input channel AN016 ADCHANNEL17 : Input channel AN017 ADCHANNEL18 : Input channel AN018 ADCHANNEL19 : Input channel AN019 ADCHANNEL20 : Input channel AN020 ADTEMPSENSOR : Extended analog input (temperature sensor output) ADINTERREFVOLT : Extended analog input (internal reference voltage) |
|
O |
uint16_t * const buffer; |
Pointer to the area where the results of conversion are stored |
[Return value]
None.