Starts SCI master transmission (simple I2C mode).
Remark 1. This API function handles SCI master transmission to the slave device at the address specified by the argument adr and the R/W#bit. SCI master transmission in byte units is repeated the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf.
Remark 2. This API function internally calls R_SCIn_IIC_StartCondition to handle processing to start SCI master transmission.
Remark 3. When performing a SCI master transmission, R_SCIn_Start must be called before this API function is called.
[Syntax]
void R_SCIn_IIC_Master_Send ( uint8_t adr, uint8_t * const tx_buf, uint16_t tx_num );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint8_t adr;  | 
    
       Slave address  | 
| 
       I  | 
    
       uint8_t * const tx_buf;  | 
    
       Pointer to a buffer storing the transmission data  | 
| 
       I  | 
    
       uint16_t tx_num;  | 
    
       Total amount of data to send  | 
[Return value]
None.