Everything

sig_sem

isig_sem

Outline
Release semaphore resource.
C format
 ER      sig_sem (ID semid);
 ER      isig_sem (ID semid);
Parameter(s)
I/O
Parameter
Description
I
 ID      semid;
ID number of the semaphore.

Explanation
These service calls releases the resource to the semaphore specified by parameter semid (adds 1 to the semaphore counter).
If a task is queued in the wait queue of the target semaphore when this service call is issued, the counter manipulation processing is not performed but the resource is passed to the relevant task (first task of wait queue).
As a result, the relevant task is unlinked from the wait queue and is moved from the WAITING state (WAITING state for a semaphore resource) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
Note With the RI600V4, the maximum possible number of semaphore resources (Maximum resource count (max_count)) is defined during configuration. If the number of resources exceeds the specified maximum resource count, this service call therefore does not release the acquired resources (addition to the semaphore counter value) but returns E_QOVR.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- semid < 0
- semid > VTMAX_SEM
E_CTX
-25
Context error.
- This service call was issued in the CPU locked state.
- The isig_sem was issued from task.
- The sig_sem was issued from non-task.
- This service call was issued in the status PSW.IPL > kernel interrupt mask level.
E_QOVR
-43
Queue overflow.
- Resource count exceeded the Maximum resource count (max_count).