CHAPTER 18 SERVICE CALLS
 The service calls provided by the RI600V4 are service routines provided for indirectly manipulating the resources (tasks, semaphores, etc.) managed by the RI600V4 from a processing program.
 act_tsk	iact_tsk	can_act	ican_act	sta_tsk	ista_tsk	ext_tsk	ter_tsk	chg_pri	ichg_pri	get_pri	iget_pri	ref_tsk	iref_tsk	ref_tst	iref_tst
 slp_tsk	tslp_tsk	wup_tsk	iwup_tsk	can_wup	ican_wup	rel_wai	irel_wai	sus_tsk	isus_tsk	rsm_tsk	irsm_tsk	frsm_tsk	ifrsm_tsk	dly_tsk
 snd_dtq	psnd_dtq	ipsnd_dtq	tsnd_dtq	fsnd_dtq	ifsnd_dtq	rcv_dtq	prcv_dtq	iprcv_dtq	trcv_dtq	ref_dtq	iref_dtq
 set_tim	iset_tim	get_tim	iget_tim	sta_cyc	ista_cyc	stp_cyc	istp_cyc	ref_cyc	iref_cyc	sta_alm	ista_alm	stp_alm	istp_alm	ref_alm	iref_alm
 rot_rdq	irot_rdq	get_tid	iget_tid	loc_cpu	iloc_cpu	unl_cpu	iunl_cpu	dis_dsp	ena_dsp	sns_ctx	sns_loc	sns_dsp	sns_dpn	vsys_dwn	ivsys_dwn	vsta_knl	ivsta_knl
 Note	 To call the service calls provided by the RI600V4 from a processing program, the header files listed below must be coded (include processing).