vrst_dtq
ER vrst_dtq (ID dtqid);
 The data having been accumulated by the data queue area are annulled. The tasks to wait to send data to the target data queue are released from the WAITING state, and EV_RST is returned as a return value for the tasks.
 Note 1	 In this service call, the tasks to wait to receive data do not released from the WAITING state.