Everything

 

-misalign [V2.04.00 or later]


This option generates an instruction string that performs a misaligned memory access.

[Specification format]

-misalign

 

[Detailed description]

-

For memory accesses, this option generates a more effective instruction string assuming that the device supports access to unaligned addresses.

-

Specifying this option more than once has the same effect as specifying it once only. No warning is output in this case.

[Remark]

-

To specify this option, enable the misaligned memory access function of the device. For details, see the user's manual of the device.