-Xcheck_exclusion_control [V1.04.00 or later]
|
This option is used to select checking of exclusive control.
[Specification format]
-Xcheck_exclusion_control=<filename>
|
- | Interpretation when omitted |
Checking of exclusive control is disabled.
[Detailed description]
- | This option loads the setting file and inserts the dbtag instruction at the specified location. |
- | This function assumes usage via CS+ and it should not be used directly by the user. |