With the CC-RH, assembler instruction can be described in the functions of a C source program.
One of the #pragma directives to embed assembler instructions is #pragma inline_asm.
This treats the function itself as an assembler instruction only, and performs inline expansion at the call site.
#pragma inline_asm ( function-specification [, function-specification]... )Note function-specification: function-name [(size=numerical value)] |
Performs inline expansion on functions coded in assembly and declared with #pragma inline_asm.
The calling conventions for an inline function with embedded assembly are the same as for ordinary function calls.
Specifying (size = numerical value) does not affect the result of compilation.
#pragma inline_asm func_add static int func_add(int a, int b){ add r6, r7 mov r7, r10 } void func(int *p){ *p = func_add(10,20); } |
If you use a register to guarantee the entrance and exit of an inline function with embedded assembly, you must save and restore this register at the beginning and end of the function. |
The compiler passes strings in #pragma inline_asm to the assembler as-is, without checking or modifying them. |
Only positive integer constants are specifiable for (size = numerical value). Specifying a floating-point number or value less than 0 will cause an error. |
If #pragma inline_asm is specified for a static function, then the function definition will be deleted after inline expansion. |
Assembly code is targeted by the preprocessor. Caution is therefore needed when using #define to define a macro with the same name as an instruction or register used in assembly language (e.g. "MOV" or "r5"). |
Although it is possible to use comments starting with a hash ("#") in RH850 assembly language, if you use this comment, do not use # comments inside functions coded in assembly, because the preprocessor will interpret these as preprocessing directives. |
#pragma inline_asm, #pragma inline, #pragma noinline, #pragma interrupt,
#pragma block_interrupt, #pragma stack_protector,
When a label is written in an assembly-language function, labels having the same name are generated for the number of times the function is expanded inline. |
In this case, take any of the following actions.
Use a local label written in the assembly language. A local label has a single name in the assembly-language code, but the assembler automatically converts it into separate names. |
When calling an assembly-language function within the current source file, define the function as static and call it only from a single location. Do not obtain the address of the assembly-language function. |
When not calling an assembly-language function within the current source file, code the function as an external function. |
The following shows a sample output code.
Outputs the specified string to the assembly-language file.
The basic format of the asm statement included in the GNU Extensions can be used.
However, the asm statement can only be used within a function. Using it outside a function will cause an error.
You can specify "volatile" or "inline" for qualifier, but they are ignored without affecting the compilation result.