Fixes the format of data records to be output.
This option is used to output an Intel HEX file or a Motorola S-record file with records of a fixed length starting from the address that has alignment with the specified number. |
The address of the first record to be output should be less than or equal to the first address of a section and be the largest number that can be divided by the specified alignment number. |
The specified numerical value or default value for the parameter of the -BYte_count option will be used as the length of the records. |
In unused areas, the value specified by the -SPace option will be output. If the -SPace option is not specified, 0x00 (with the -CRc option not specified) or 0xff (with the -CRc option specified) as the default value will be output. |
Starting the output of records from an address that can be divided by 8, with the length of each record fixed to 16 bytes (10 in hexadecimal). |