-SPLIT_VECT [V1.07 or later]
|
This option generates vector table sections split by vector table address.
[Specification format]
- | Interpretation when omitted |
None
[Detailed description]
- | This option generates vector table sections split by vector table address. |
- | A vector table section is not generated for an unused area of the vector table address. |
[Example of use]
- | To generate a vector table section ".vect14" for vector table address 0x14, code as: |
>rlink a.obj b.obj -vectn=14=__dummy -split_vect
|
[Remark]
- | If the -vect option is specified, this option will be invalid. |
- | If the -form={object | relocate | library} option, -strip option, or -extract option is specified, this option will be invalid. |