Everything
3.2.2 Header information

The version information of the optimizing linker and the time of linkage are output.

The output example of the header information is shown below.

Renesas Optimizing Linker (VX.XX.XX)            XX-Xxx-XXXX XX:XX:XX    (1)

Number

Description

(1)

Version information of the optimizing linker and time of linkage

The version information of the optimizing linker and the time of linkage are output.