Option strings specified by a command line or subcommand file are output.
The output example of the option information when the following command line and subcommand file are specified is shown below.
<Command line>
>rlink -subcommand=sub.txt -list -show
|
<Subcommand file "sub.txt">
*** Options ***
-subcommand=sub.txt (1)
input sample.obj (2)
-list (1)
-show (1)
|
|
|
|
Options specified by command line
The options specified by the command line are output (in their specified order).
|
|
Options specified in subcommand file
The options specified in subcommand file "sub.txt" are output.
|