Everything
7.5.3 Functions for greatest-width integer types

The functions for greatest-width integer types are as follows.

Table 7.5

Functions for Greatest-Width Integer Types

Function Name

Outline

imaxabs [V1.07 or later]

Output of absolute value (intmax_t type) (C99)

imaxdiv [V1.07 or later]

Division (intmax_t type) (C99)

strtoimax [V1.07 or later]

Conversion of character string to integer (intmax_t type) and storing pointer to last character string (C99)

strtoumax [V1.07 or later]

Conversion of character string to integer (uintmax_t type) and storing pointer to last character string (C99)