Non-local jump functions are as follows.
Table 7.7
Non-Local Jump Functions
Function/Macro Name
Outline
setjmp
Save the environment in which a function call was made
longjmp
Restore the environment in which a function call was made