Hyperbolic tangent
[Classification]
Mathematical library
[Syntax]
#include <math.h>
float   __far   tanhf(float x);
[Return value]
Returns the hyperbolic tangent of x.
If the solution is a denormal number,  tanhf sets macro ERANGE to global variable errno.
[Description]
This function calculates the hyperbolic tangent of x.  Specify the angle in radian.  The definition expression is as follows.
 
sinhf (x) / coshf (x)