Obtain the logarithm with a base of 10
Returns the logarithm of x with base 10.
log10 returns a Not-a-Number (NaN) and sets macro EDOM to global variable errno if x is negative.
If x is zero, it returns -∞ and sets macro ERANGE to global variable errno.