Everything

longjmp


Restore the environment in which a function call was made

[Classification]

Standard library

[Syntax]

#include <setjmp.h>

typedef int __near jmp_buf[3];

void __far longjmp(jmp_buf env, int val);

[Description]

This function performs a non-local jump to the place immediately after setjmp using env saved by setjmp.