This tab displays the initialize routine information (e.g. Start Address and Extended Information) of the RI78V4.
 
 Figure A-20.    [Initialize Routine] Tab
 
 The following items are explained here.
 
 -	 From the [Debug] menu, select [Download].
 
 -	 From the [View] menu, select [Realtime OS] >> [Resource Information].
 
 [Description of each area]
 
 (1)	 Information display area
 
 This area displays the initialize routine information (e.g. Start Address and Extended Information) of the RI78V4.
 
 This area consists of the following items.
 
 
  
  
    | 
 | 
    
 An icon and the start address of the initialize routine are shown in the following format.
  
 | 
  
  
    | 
 | 
    
 | 
  
  
    | 
 | 
    
 | 
  
 
 Remark	 If the initialize routine information (e.g. Start Address and Extended Information) in each cell is double clicked, then Editor panel displays the source file of the initialize routine, and the caret moves to the corresponding location.
 
 The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
 
 
  
  
    | 
 | 
    
 Displays cascade menus for selecting the header items to display.
  
 | 
  
  
    | 
 | 
    
 | 
    
 The following items are displayed for selection.
  
 Start Address, Extended Information, Attribute
  
 | 
  
  
    | 
 | 
    
 | 
    
 | 
    
 The item in question will be displayed.
  
 | 
  
  
    | 
 | 
    
 The item in question will not be displayed.
  
 | 
  
  
    | 
 | 
    
 Displays cascade menus for selecting the display notation.
  
 | 
  
  
    | 
 | 
    
 | 
    
 The following items are displayed for selection.
  
 Start Address, Extended Information
  
 | 
  
  
    | 
 | 
    
 Displays value in signed decimal number.
  
 | 
  
  
    | 
 | 
    
 Displays value in hexadecimal number.
  
 | 
  
 
 
  
  
    
 Jump to Source (Start Address)
  
 | 
    
 Opens the Editor panel, and displays the source code of the initialize routine.
  
 | 
  
  
    
 Jump to Disassemble (Start Address)
  
 | 
    
 Opens the Disassemble panel, and displays the results of disassembling the initialize routine.
  
 | 
  
  
    | 
 | 
    
 Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).
  
 |