This tab displays the ready queue information (e.g. Priority and Number of Tasks) of the RI78V4.
Figure A-21. [Ready Queue] Tab
The following items are explained here.
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This layer displays the ready queue information (e.g. Priority and Number of Tasks) of the RI78V4.
This layer consists of the following items.
|
An icon indicating the current status of the ready queue and the task priority are shown in the following format.
|
|
|
|
There are no queued tasks.
|
|
The total number of queued tasks (tasks with of READY state or RUNNING state) is shown.
|
The executing task information (e.g. Task Name and ID) only appears if there are tasks queued in the ready queue.
See the
[Task] tab for details about executing task information.
Figure A-22. [Ready Queue] Tab (Executing Task Information)
Remarks 1.
If the executing task information (Task Name, ID, Status, Wait Factor, Wait Data, Time Left, Interrupt, Current Priority, Task Start Address, Current PC) in each cell is double clicked, then Editor panel displays the source file of the task, and the caret moves to the corresponding location.
2. If the executing task information (Current Task SP) in the cell is double clicked, then Memory panel displays the contents of the task stack, and the caret moves to the corresponding location.
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
|
Displays cascade menus for selecting the header items to display.
|
|
|
The following items are displayed for selection.
Priority, Number of Tasks
|
|
The item in question will be displayed.
|
|
The item in question will not be displayed.
|
|
Displays cascade menus for selecting the display notation.
|
|
|
The following items are displayed for selection.
Priority, Number of Tasks
|
|
Displays value in signed decimal number.
|
|
Displays value in hexadecimal number.
|
|
Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).
|