Everything
Everything
top
RH850 Debug Tool
FUNCTIONS
Configuration of Operating Environment of the Debug Tool
2.3
Configuration of
Operating Environment of the Debug Tool
This section describes the configuration of the operating environment for each debug tool.
To the latest version of this page
Differences Information
Previous Topic
[Simulator]
Next Topic
Select the debug tool to use
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Select the debug tool to use
[Full-spec emulator]/[IE850A]/[E1]/[E20]/[E2]/[E2 Lite]
[Simulator]
Applicable Debugging Methods
Connect to/Disconnect from the Debug Tool
Download/Upload Programs
Display/Change Programs
Usage of PIC/PID Function
Select a Core (PE)
Execute Programs
Stop Programs (Break)
Display/Change the Memory, Register and Variable
Display Information on Function Call from Stack
Collect Execution History of Programs
Measure Execution Time of Programs
Measure Performance [Full-spec emulator][E1][E20]
Measure Coverage [Simulator]
Set an Action into Programs
Manage Events
Use Hook Function
About Input Value
Saving and Restoring the States of Debug Tools
Exclusive Control Checking Tool
Pseudo-error Debugging [Full-spec emulator][E1][E2][E2 Lite][E20]
Debugging CAN Bus Reception Procedures [Full-spec emulator][E1][E2][E2 Lite][E20]
Measuring CAN Bus Reception Processing Times [E2]