This section describes how to display and change programs when a load module file with the debug information is downloaded to a debug tool.
Downloaded programs can be displayed in the following panels.
| Editor panel | 
| Disassemble panel | 
| It is normally necessary to download a load module file with debugging information in order to perform the source level debugging, but it is also possible to do so by downloading an Intel HEX file (*.hex), Motorola S-record file (*.mot), or binary file (*.bin) (see "2.6.2.4 Perform source level debugging with files other than the load module file format"). |