-show=xreferenceを指定した場合、シンボルの参照情報(クロスリファレンス情報)を出力します。
| *** Cross Reference List *** (1) (2) (3) (4) (5) No Unit Name Global.Symbol Location External Information 0001 a SECTION=P _func 00000100 _func1 00000116 _main 0000012c _g 00000136 SECTION=B _a 00000190 0001(00000140:P) 0002(00000178:P) 0003(0000018c:P) 0002 b SECTION=P _func01 00000154 0001(00000148:P) _func02 00000166 0001(00000150:P) 0003 c SECTION=P _func03 00000184 | 
| -form=relocate指定時は、セクション先頭からの相対値となる | |