文字列を整数(uintmax_t型)へ変換し,最終文字列へのポインタを格納します。
uintmax_t __far strtoumax(const char __near * restrict nptr, char __near * __near * restrict endptr, int base);(C99)
uintmax_t __far _COM_strtoumax_ff(const char __far * restrict nptr, char __far * __far * restrict endptr, int base);(C99)
部分文字列が変換できた場合,変換された値を返します。変換できなかった場合,0を返します。
オーバフローが生じる場合,UINTMAX_MAXを返し,マクロERANGEをグローバル変数errnoに設定します。
nptrの指す文字列の先頭から0個以上の空白類文字(isspace関数が真となる文字)の列を読み飛ばし,次の文字からの文字列をuintmax_t型の表現に変換します。baseが0である場合はCの基数表現と解釈し,baseが2以上36以下である場合はその値を基数とします。endptrがnullポインタでない場合は変換されなかった残りの文字列へのポインタをendptrに設定します。