char __near * __far strcat(char __near *s1, const char __near *s2);(C90)
char __near * __far strcat(char __near * restrict s1, const char __near * restrict s2);(C99) 【V1.07以降】
char __far * __far _COM_strcat_ff(char __far *s1, const char __far *s2);(C90)
char __far * __far _COM_strcat_ff(char __far * restrict s1, const char __far * restrict s2);(C99) 【V1.07以降】
s2の指す文字列のコピーを,null文字(\0)を含めて,s1の指す文字列の末尾に連結します。s2の最初の文字はs1の終わりのnull文字(\0)を上書きします。