#include <machine.h>
#include <_h_c_lib.h>
//#include <stddef.h> // Remove the comment when you use errno
//#include <stdlib.h> // Remove the comment when you use rand()
#include "typedefine.h" // Define Types
#include "stacksct.h" // Stack Sizes (Interrupt and User)
#ifdef __cplusplus // For Use Reset vector
extern "C" {
#endif
void PowerON_Reset_PC(void);
void main(void);
#ifdef __cplusplus
}
#endif
#ifdef __cplusplus // For Use SIM I/O
extern "C" {
#endif
extern void _INIT_IOLIB(void);
extern void _CLOSEALL(void);
#ifdef __cplusplus
}
#endif
#define PSW_init 0x00010000 // PSW bit pattern
#define FPSW_DPSW_init 0x00000000 // FPSW/DPSW bit base pattern
//extern void srand(_UINT); // Remove the comment when you use rand()
//extern _SBYTE *_s1ptr; // Remove the comment when you use strtok()
//#ifdef __cplusplus // Use Hardware Setup
//extern "C" {
//#endif
//extern void HardwareSetup(void);
//#ifdef __cplusplus
//}
//#endif
//#ifdef __cplusplus // Remove the comment when you use global class object
//extern "C" { // Sections C$INIT and C$END will be generated
//#endif
//extern void _CALL_INIT(void);
//extern void _CALL_END(void);
//#ifdef __cplusplus
//}
//#endif
#pragma section ResetPRG // output PowerON_Reset_PC to PResetPRG section
#pragma entry PowerON_Reset_PC
void PowerON_Reset_PC(void)
{
#if (__RX_ISA_VERSION__ >= 2) || defined(__RXV2)
set_extb(__sectop("EXCEPTVECT")); // Remove the comment when you want to set an address
// into the Exception Vector Table Register of RXv2 or later
|