2.6.1 Set the columns to display

You can show or hide any of the items (columns) displayed on the Function List panel/Variable List panel.

 

(1) Restricting the columns displayed

(2) Adding columns to display

(1)

Restricting the columns displayed

There are two ways to perform this operation, as shown below.

(a)

Performing the operation from the panel

Use the mouse to drag and drop the items to hide off of the panel.

Figure 2.9

Restricting Columns Displayed (Operation from Panel)

(b)

Performing the operation from the Column Chooser dialog box

On the left edge of the panel's header area, click the button to open the Column Chooser dialog box, and then clear the check boxes of the names of the items to hide.

Figure 2.10

Restricting Columns Displayed (Operation from Column Chooser Dialog Box)

(2)

Adding columns to display

On the left edge of the panel's header area, click the button to open the Column Chooser dialog box, and then select the check boxes of the names of the columns to display, or drag and drop them directly from the dialog box to the information display area on the panel using the mouse.

Figure 2.11

Adding Columns to Display (Clearing Check Boxes in Column Chooser Dialog Box)

Figure 2.12

Adding Columns to Display (Dragging and Dropping from Column Chooser Dialog Box)