R_RTC_Get_CalendarCounterValue


Reads the counter value of the real-time clock.(in the case of the calendar mode setting)

[Syntax]

#include    "r_cg_macrodriver.h"
#include    "r_cg_rtc.h"
MD_STATUS   R_RTC_Get_CalendarCounterValue ( rtc_counter_value_t * const counter_read_val );

[Argument(s)]

I/O

Argument

Description

O

rtc_counter_value_t
  * const counter_read_val;

Pointer to structure in which to store the counter value being read

Remark

See R_RTC_Set_CounterValue for details about the rtc_counter_value_t counter value.

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR

Read failure