R_RTC_Get_BinaryAlarmValue


Reads the alarm conditions (weekday, hour, minute).(in the case of the binary mode setting)

[Syntax]

#include    "r_cg_macrodriver.h"
#include    "r_cg_rtc.h"
void R_RTC_Get_BinaryAlarmValue ( uint32_t * const alarm_enable, uint32_t * const
alarm_val );

[Argument(s)]

I/O

Argument

Description

O

uint32_t * const alarm_enable

Pointer to structure in which to store the alarm enable value being read

O

uint32_t * const alarm_val

Pointer to structure in which to store the conditions being read

[Return value]

None.