R_RTC_Set_CalendarAlarmOn


Starts the alarm interrupt function.(in the case of the calendar mode setting)

[Syntax]

#include    "r_cg_macrodriver.h"
#include    "r_cg_rtc.h"
void    R_RTC_Set_CalendarAlarmOn ( uint8_t enb_set );

[Argument(s)]

 

I/O

Argument

Description

I

uint8_t enb_set;

Alarm enable

Remark

Below is shown the structure enb_set.

[Return value]

None.