Everything
2.4.5 Change the project name

You can change the name of the project (main project or subproject) on the project tree.

Select the Project node or Subproject node and select [Rename] on the context menu.

Figure 2.22

[Rename] Item (For a Project)

 

Remark

After changing the project name, when you save the project, the actual name of the project file is also changed.