Everything
2.4.2 Add an existing subproject

Select the Project node on the project tree and if you select [Add] >> [Add Subproject...] on the context menu, the Add Existing Subproject dialog box will open.

Figure 2.18

Add Existing Subproject Dialog Box

 

On the dialog box, specify the subproject file of the subproject to add and click the [Open] button.