Everything

 

-COmpress


This option compresses the debug information.

[Specification format]

-COmpress

 

-

Interpretation when omitted

The debug information is not compressed (It is the same result as when the -nocompress option is specified).

[Detailed description]

-

This option compresses the debug information.

-

By compressing the debug information, the loading speed of the debugger is improved.

[Example of use]

-

To compress the debug information, describe as:

>rlink a.obj b.obj -output=c.abs -compress

[Remark]

-

If the -form={object|relocate|library|hexadecimal|stype|binary} option or -strip option is specified, this option will be invalid.