Everything

 

-EXTract


This option extracts library modules.

[Specification format]

-EXTract=module[,module]...

 

-

Interpretation when omitted

None

[Detailed description]

-

This option extracts library module module from the library file specified by the -library option.

[Example of use]

-

To extract module "file1" from library file "lib.lib" and output it to a file with the object file output format, describe as:

>rlink -library=lib1.lib -extract=file1 -form=obj

[Remark]

-

If the -form={absolute|hexadecimal|stype|binary} option and the -strip option is specified, this option will be invalid.

-

When the -form=library option is specified, library modules can be deleted.

-

When the -form={absolute|relocate|hexadecimal|stype|binary} option is specified, external symbols can be deleted.