Everything
2.3.2 [E1]

Configure the operating environment on the Property panel below when using E1.

Note that the contents of the Property panel differ depending on the communication method (FINE communications [E1(Serial)] or JTAG communications [E1(JTAG)]) between E1 and the target system.

Figure 2.6

Property Panel [E1(Serial)]

Figure 2.7

Property Panel [E1(JTAG)]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.2.1 [Connect Settings] tab

2.3.2.2 [Debug Tool Settings] tab

2.3.2.3 [Download File Settings] tab

2.3.2.4 [Hook Transaction Settings] tab