Everything
2.3.3 [E20]

Configure the operating environment on the Property panel below when using E20.

Note that the contents of the Property panel differ depending on the communication method (FINE communications [E20(Serial)] or JTAG communications [E20(JTAG)]) between E20 and the target system.

Figure 2.25

Property Panel [E20(Serial)]

Figure 2.26

Property Panel [E20(JTAG)]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.3.1 [Connect Settings] tab

2.3.3.2 [Debug Tool Settings] tab

2.3.3.3 [Download File Settings] tab

2.3.3.4 [Hook Transaction Settings] tab